i.MX7d bare-metal example code for linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7d bare-metal example code for linux

2,010 Views
vineetanarkhede
Contributor I

Hi,

I want bare-metal example code to read ADC in continuous mode (with cortex A7 processor in i.MX7d), using IMX7 SABRE board and linux PC.

Below are the queries regarding this,

1. Is there any bare-metal example code available for IMX7 SABRE?

2. If it is available, which build environment is required?

3. I have downloaded one BSP from below link, but the adc example code available there is for cortex M4,how to run it on cortex A7?

https://community.nxp.com/thread/448268
https://www.nxp.com/webapp/sps/download/preDownload.jsp
Labels (1)
0 Kudos
Reply
1 Reply

1,719 Views
igorpadykov
NXP Employee
NXP Employee

Hi vineeta

one can look at i.MX 7Dual/Solo FreeRTOS BSP for Cortex-M4, please check

included in package documentation describing how to complile and run M4 applications

https://www.nxp.com/webapp/Download?colCode=FreeRTOS_iMX7D_1.0.1_WIN&appType=license&location=null&P... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply