i.MX7d bare-metal example code for linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7d bare-metal example code for linux

2,056件の閲覧回数
vineetanarkhede
Contributor I

Hi,

I want bare-metal example code to read ADC in continuous mode (with cortex A7 processor in i.MX7d), using IMX7 SABRE board and linux PC.

Below are the queries regarding this,

1. Is there any bare-metal example code available for IMX7 SABRE?

2. If it is available, which build environment is required?

3. I have downloaded one BSP from below link, but the adc example code available there is for cortex M4,how to run it on cortex A7?

https://community.nxp.com/thread/448268
https://www.nxp.com/webapp/sps/download/preDownload.jsp
ラベル(1)
0 件の賞賛
返信
1 返信

1,765件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vineeta

one can look at i.MX 7Dual/Solo FreeRTOS BSP for Cortex-M4, please check

included in package documentation describing how to complile and run M4 applications

https://www.nxp.com/webapp/Download?colCode=FreeRTOS_iMX7D_1.0.1_WIN&appType=license&location=null&P... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信