i.MX7S + LPDDR2 : Wr/Rd Problem in DDR Test Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7S + LPDDR2 : Wr/Rd Problem in DDR Test Tool

1,628件の閲覧回数
davidgeorge
Contributor III

I have a custom board with i.MX7S and Micron LPDDR2 (1GB in 2 Ranks, 32 bit).

I have created the DDR register values with NXP's 'i.MX7D DDR Controller Configuration Spreadsheet '

When I run the DDR Stress Test Tools;

1) The Calibration Passes @ 460 MHz - I get delay values with a good margin

2) The Stress Test runs @ 460 MHz overnight without error.

However when I try a Memory Write & Read it only writes successfully ONCE. After that I can't write another value, it always reads the same value, if I do a Calibration cycle then I can Write just one value again.

So obviously something is setup wrong or not configured correctly.

Can anyone help or has experience for using LPDDR2 with i.MX7?

Thanks

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,372件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The following is good place to continue discussion with DDR Stress Test designers.

i.MX6/7 DDR Stress Test Tool V2.60 

Please try the recent release of "ddr_stress_tester_v2.60.zip".

Regards,

Yuri.

0 件の賞賛
返信