i.MX7D power-down sequence issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D power-down sequence issue

1,238件の閲覧回数
felixhsu
Contributor III

Hi All

The i.MX7D had power-down sequence,  but customer power-down direct use AC power off, about i.MX7D use AC power off design on the power-down have any concern of side effect?

pastedImage_1.png

pastedImage_2.png

ラベル(5)
0 件の賞賛
返信
1 返信

1,082件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  It is highly recommended to follow the power-down sequence, specified ini.MX datasheet(s) :

The system design must comply with power-up sequence, power-down sequence, and steady state
guidelines as described in this section to guarantee the reliable operation of the device. Any deviation
from these sequences may result in the following situations:
• Excessive current during power-up phase
• Prevention of the device from booting

• Irreversible damage to the processor (worst-case scenario)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信