i.MX7D application without DRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7D application without DRAM

697 次查看
chris_f
Contributor V

Is it possible to use the iMX7D without any DRAM? NVCC_DRAM is required ON in the RUN mode according to IMX7DCEC table 14. Will the device enter RUN mode without this? If NVCC_DRAM is required, does there actually need to be any DRAM attached to enter RUN mode?

标签 (1)
0 项奖励
回复
1 回复

622 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

 It is possible to use the iMX7D without any DRAM, at least in theory,

when user applications do not require much memory. Usually it is

bare metal codes, working without OS support.

  In any case i.MX7 NVCC_DRAM must be applied.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复