i.MX7D Clock voltage level issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D Clock voltage level issue

ソリューションへジャンプ
1,666件の閲覧回数
felixhsu
Contributor III

Hi All

The CCM_EXT_CLK2 of the i.MX7D clock voltage level how much do it need, it is 3.3V or 1.8V, thanks.

pastedImage_1.png

ラベル(2)
0 件の賞賛
返信
1 解決策
1,531件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

It need 3.3V. You can refer to the IMX7DCEC.pdf,section 4.11.2.6 Bus operation condition for 3.3 V and 1.8 V signaling
The DC parameters for the NVCC_SD1, NVCC_SD2 and NVCC_SD3 supplies are
identical to those shown in Table 29, "GPIO DC Parameters," on page 44.

pastedImage_3.png

And in the datasheet you can see the follow functions

pastedImage_1.png
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,531件の閲覧回数
felixhsu
Contributor III

Hi Rita

Voltage level of the CCM_EXT_CLK2 will follow GPIO calculation formula is right?

My mean is the VIH of CCM_EXT_CLK2 minimal is OVDDx0.7 and VIL maximal is OVDDx0.3.

Thanks.

0 件の賞賛
返信
1,532件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

It need 3.3V. You can refer to the IMX7DCEC.pdf,section 4.11.2.6 Bus operation condition for 3.3 V and 1.8 V signaling
The DC parameters for the NVCC_SD1, NVCC_SD2 and NVCC_SD3 supplies are
identical to those shown in Table 29, "GPIO DC Parameters," on page 44.

pastedImage_3.png

And in the datasheet you can see the follow functions

pastedImage_1.png
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信