i.MX7 USB Low Power Boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 USB Low Power Boot.

Jump to solution
1,632 Views
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX7 USB Low Power Boot.
Please see chapter 6.6.11 in IMX7DSRM Rev.0.1.
They want to know whether i.MX7 always enters USB Low Power Boot if LPB_BOOT=10b or 11b.


I understand it is not always, but if satisfied Figure 6-46 flow, there is a possibility to enter to USB Low Power Boot even if enough power is supplied from PMIC.
Is my understanding correct?


Best Regards,
Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,435 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Generally Your understanding is correct. Also, please take into account, that 

"If LPB_BOOT fuses are blown, the Chip will check if there is low power condition via
GPIO_3 pad. [...] Polarity of low power boot condition on GPIO_3 pad is set
by BT _LPB_POLARITY fuse. "

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,436 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Generally Your understanding is correct. Also, please take into account, that 

"If LPB_BOOT fuses are blown, the Chip will check if there is low power condition via
GPIO_3 pad. [...] Polarity of low power boot condition on GPIO_3 pad is set
by BT _LPB_POLARITY fuse. "

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply