i.MX7 EIM asynchronous timing parameters

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7 EIM asynchronous timing parameters

1,268 次查看
ko-hey
Senior Contributor II

Hi all

I want to know how to calculate the EIM asynchronous timing parameters which are shown in table 39 in MX7SCEC.

pastedImage_2.png

The parameter of CSA which include WCSA and RCSA is defined as below.

pastedImage_3.png

From above, when user set RCSA to "111", the Max of WE31 is -4 ns.

Am I correct ?

How can I calculate the parameters ?

Ko-hey

标签 (2)
0 项奖励
回复
3 回复数

1,161 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

not sorry, as CSA (RCSA) should be entered to formula in EIM clock cycles

expressed in ns units.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,161 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for reply.

For 135MHz, the cycle is 7.4 ns and CSA is 7.

The Max of WE31 is 3 - (7 x EIM clock cycle) = 3 - 7 * 7.4 = -48.8 ns

Am I correct ?

If the above is correct, I think most of them will be minus regulations.

Ko-hey

0 项奖励
回复

1,161 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is correct however there restrictions on max. EIM frequency
given in Table 45. EIM bus timing parameters i.MX7D Datasheet
htttp://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf

minus is because CS is delayed.

Best regards
igor

0 项奖励
回复