i.MX7 Android Browser

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7 Android Browser

ソリューションへジャンプ
2,741件の閲覧回数
ryanschaefer
Contributor IV

I am testing android on the i.mx7 sabresd platform. The built-in browser is not built when building for sabresd_7d-eng. I noticed that one of the patches excludes the browser because it relies on OpenGL, and the i.mx7d does not have OGL support (or a GPU). I have removed the check in packages/apps/Browser/Android.mk, and was able to include the browser in my build.

The browser unfortunately crashes with the error :

"chromium: [FATAL:gl_surface_android.cc(58)] Check failed: kGLImplementationNone != GetGLImplementation() (0 vs. 0)"

Is there a way to include a OGL software renderer on android? I realize that without a GPU, this could be painfully slow performance wise.

Thanks,

Ryan

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,244件の閲覧回数
ryanschaefer
Contributor IV

After more research - Android includes a software rendering solution for OpenGL (PixelFlinger), but this only supports up to OpenGL 1.1 I believe. PixelFlinger may have been removed from newer releases - I'm still unsure about this. OpenGL 2.0 is required for many android packages. For example, the built-in browser (and chrome, who both use chromium webengine under the hood), or any app that tries to use WebViews currently crash.

元の投稿で解決策を見る

2 返答(返信)
2,245件の閲覧回数
ryanschaefer
Contributor IV

After more research - Android includes a software rendering solution for OpenGL (PixelFlinger), but this only supports up to OpenGL 1.1 I believe. PixelFlinger may have been removed from newer releases - I'm still unsure about this. OpenGL 2.0 is required for many android packages. For example, the built-in browser (and chrome, who both use chromium webengine under the hood), or any app that tries to use WebViews currently crash.

2,244件の閲覧回数
b36401
NXP Employee
NXP Employee

Our Android BSP for i.MX7 does not support OpenGL.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信