i.MX6quad sabre-sd board interface testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6quad sabre-sd board interface testing

1,280 Views
jayalakshmi1
Contributor I

May I know where can I get the peripheral components (i.e. LVDS, camera module etc.) for interfacing with the MCIMX6Q-SDB..??

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,146 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

one can look at differencies between two boards

https://www.nxp.com/docs/en/fact-sheet/RDIMX6SABREBRDFS.pdf 

LVDS panel
MCIMX-LVDS1 Product Information|NXP 
SEIKO-WVGA panel
MCIMX28LCD Product Information|NXP 

for camera one search on community, for example

Are cameras included in the iMX6Q SDP Kit?https://community.nxp.com/message/320993?commentID=320993#comment-320993 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply