Are cameras included in the iMX6Q SDP Kit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are cameras included in the iMX6Q SDP Kit?

ソリューションへジャンプ
4,053件の閲覧回数
makislivadas
Contributor IV

Need to know if cameras are included in this kit.

SABRE Platform for Smart Devices Based on the i.MX 6 Series Product Summary Page

According to this document

https://community.freescale.com/servlet/JiveServlet/previewBody/93975-102-3-4139/ov5642-mx6qsdp-stre...

There are two suitable kits featured in the kit but is not clear to me if the cameras are included.

Anybody bought this kit here that can confirm the cameras are included?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,908件の閲覧回数
hippo
NXP TechSupport
NXP TechSupport

The Smart Device Platform (MCIMX6Q-SDP) include both MIPI OV5640 and CSI OV5642 modules. Customer doesn't need to buy additional module for MCIMX6Q-SDP.

For the MCIMX6Q-SDB, it only provides the CSI OV5642 module. If the customers want to use the MIPI camera on this board, they need to soldering the interface of the board by themselves then connect OV5642.

For the schematics, you can refer to MCIMX6Q-SDP's.

You may find this module with Part Numbers OV05640-MRFL-A00A/ OV5462-MRSL-A01A from vendor A-Kerr (http://www.a-kerr.com/en/content.php?cid=about). Other vendors might have similar components but these are the ones used on our SABRE Platforms.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,909件の閲覧回数
hippo
NXP TechSupport
NXP TechSupport

The Smart Device Platform (MCIMX6Q-SDP) include both MIPI OV5640 and CSI OV5642 modules. Customer doesn't need to buy additional module for MCIMX6Q-SDP.

For the MCIMX6Q-SDB, it only provides the CSI OV5642 module. If the customers want to use the MIPI camera on this board, they need to soldering the interface of the board by themselves then connect OV5642.

For the schematics, you can refer to MCIMX6Q-SDP's.

You may find this module with Part Numbers OV05640-MRFL-A00A/ OV5462-MRSL-A01A from vendor A-Kerr (http://www.a-kerr.com/en/content.php?cid=about). Other vendors might have similar components but these are the ones used on our SABRE Platforms.

0 件の賞賛
返信
2,908件の閲覧回数
pieterpostma
Contributor I

I bought the SDB and there is NO camera module. I also can't find it on the a-kerr.com.

Are there alternatives? Are there other compatible camera's for the sabre SDB?

0 件の賞賛
返信