i.MX6q PCIe mem assign errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6q PCIe mem assign errors

3,055 次查看
aden
Contributor I

Hello,

I am trying to interface with PLX switch ic and 4 FPGAs using PCIe.

During pcie bring up sequence, I got memory assign errors as follows.

How can I increase pcie mem space?

Kernel 3.0.35

root@freescale ~$ lspci                                                   
00:00.0 Class 0604: 16c3:abcd                                             
01:00.0 Class 0604: 10b5:8624                                             
02:01.0 Class 0604: 10b5:8624                                             
02:04.0 Class 0604: 10b5:8624                                             
02:05.0 Class 0604: 10b5:8624                                             
02:06.0 Class 0604: 10b5:8624                                             
02:08.0 Class 0604: 10b5:8624                                             
02:09.0 Class 0604: 10b5:8624                                             
05:00.0 Class 1180: 1b03:7800                                             

06:00.0 Class 1180: 1b03:7800

I got follow dmesg

root@freescale ~$ dmesg | grep pci                                        
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.                     
PCIE: imx_pcie_pltfm_probe start link up.                                 
pci 0000:00:00.0: [16c3:abcd] type 1 class 0x000604                       
pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff 64bit pref]          
pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]                
pci 0000:00:00.0: supports D1                                             
pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold                  
pci 0000:00:00.0: PME# disabled                                           
pci 0000:01:00.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:01:00.0: reg 10: [mem 0x00000000-0x0001ffff]                     
pci 0000:01:00.0: PME# supported from D0 D3hot D3cold                     
pci 0000:01:00.0: PME# disabled                                           
pci 0000:02:01.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:01.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:01.0: PME# disabled                                           
pci 0000:02:04.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:04.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:04.0: PME# disabled                                           
pci 0000:02:05.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:05.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:05.0: PME# disabled                                           
pci 0000:02:06.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:06.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:06.0: PME# disabled                                           
pci 0000:02:08.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:08.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:08.0: PME# disabled                                           
pci 0000:02:09.0: [10b5:8624] type 1 class 0x000604                       
pci 0000:02:09.0: PME# supported from D0 D3hot D3cold                     
pci 0000:02:09.0: PME# disabled                                           
pci 0000:05:00.0: [1b03:7800] type 0 class 0x001180                       
pci 0000:05:00.0: reg 10: [mem 0x00000000-0x0003ffff]                     
pci 0000:05:00.0: reg 14: [mem 0x00000000-0x007fffff]                     
pci 0000:05:00.0: reg 18: [mem 0x00000000-0x007fffff]                     
pci 0000:05:00.0: reg 1c: [mem 0x00000000-0x00ffffff]                     
pci 0000:05:00.0: reg 20: [mem 0x00000000-0x01ffffff]                     
pci 0000:06:00.0: [1b03:7800] type 0 class 0x001180                       
pci 0000:06:00.0: reg 10: [mem 0x00000000-0x0003ffff]                     
pci 0000:06:00.0: reg 14: [mem 0x00000000-0x007fffff]                     
pci 0000:06:00.0: reg 18: [mem 0x00000000-0x007fffff]                     
pci 0000:06:00.0: reg 1c: [mem 0x00000000-0x00ffffff]                     
pci 0000:06:00.0: reg 20: [mem 0x00000000-0x01ffffff]                     
pci 0000:00:00.0: BAR 8: can't assign mem (size 0x8a00000)                
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref]  

pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI add)

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]        
pci 0000:01:00.0: BAR 8: can't assign mem (size 0x8800000)                
pci 0000:01:00.0: BAR 0: can't assign mem (size 0x20000)                  
pci 0000:02:05.0: BAR 8: can't assign mem (size 0x4400000)                
pci 0000:02:06.0: BAR 8: can't assign mem (size 0x4400000)                
pci 0000:02:01.0: PCI bridge to [bus 03-03]                               
pci 0000:02:01.0:   bridge window [io  disabled]                          
pci 0000:02:01.0:   bridge window [mem disabled]                          
pci 0000:02:01.0:   bridge window [mem pref disabled]                     
pci 0000:02:04.0: PCI bridge to [bus 04-04]                               
pci 0000:02:04.0:   bridge window [io  disabled]                          
pci 0000:02:04.0:   bridge window [mem disabled]                          
pci 0000:02:04.0:   bridge window [mem pref disabled]                     
pci 0000:05:00.0: BAR 4: can't assign mem (size 0x2000000)                
pci 0000:05:00.0: BAR 3: can't assign mem (size 0x1000000)                
pci 0000:05:00.0: BAR 1: can't assign mem (size 0x800000)                 
pci 0000:05:00.0: BAR 2: can't assign mem (size 0x800000)                 
pci 0000:05:00.0: BAR 0: can't assign mem (size 0x40000)                  
pci 0000:02:05.0: PCI bridge to [bus 05-05]                               
pci 0000:02:05.0:   bridge window [io  disabled]                          
pci 0000:02:05.0:   bridge window [mem disabled]                          
pci 0000:02:05.0:   bridge window [mem pref disabled]                     
pci 0000:06:00.0: BAR 4: can't assign mem (size 0x2000000)                
pci 0000:06:00.0: BAR 3: can't assign mem (size 0x1000000)                
pci 0000:06:00.0: BAR 1: can't assign mem (size 0x800000)                 
pci 0000:06:00.0: BAR 2: can't assign mem (size 0x800000)                 
pci 0000:06:00.0: BAR 0: can't assign mem (size 0x40000)                  
pci 0000:02:06.0: PCI bridge to [bus 06-06]                               
pci 0000:02:06.0:   bridge window [io  disabled]                          
pci 0000:02:06.0:   bridge window [mem disabled]                          
pci 0000:02:06.0:   bridge window [mem pref disabled]                     
pci 0000:02:08.0: PCI bridge to [bus 07-07]                               
pci 0000:02:08.0:   bridge window [io  disabled]                          
pci 0000:02:08.0:   bridge window [mem disabled]                          
pci 0000:02:08.0:   bridge window [mem pref disabled]                     
pci 0000:02:09.0: PCI bridge to [bus 08-08]                               
pci 0000:02:09.0:   bridge window [io  disabled]                          
pci 0000:02:09.0:   bridge window [mem disabled]                          
pci 0000:02:09.0:   bridge window [mem pref disabled]                     
pci 0000:01:00.0: PCI bridge to [bus 02-08]                               
pci 0000:01:00.0:   bridge window [io  disabled]                          
pci 0000:01:00.0:   bridge window [mem disabled]                          
pci 0000:01:00.0:   bridge window [mem pref disabled]                     
pci 0000:00:00.0: PCI bridge to [bus 01-08]                               
pci 0000:00:00.0:   bridge window [io  disabled]                          
pci 0000:00:00.0:   bridge window [mem disabled]                          

pci 0000:00:00.0:   bridge window [mem pref disabled]  

Best regards

标签 (1)
0 项奖励
回复
4 回复数

1,902 次查看
aden
Contributor I

Hi,

We tried to modify the kernel source to increase PCIE Memory regions as follows

PCIE_ARB_BASE_ADDR and PCIE_ARB_END_ADDR in mx6.h.

/* CPU Memory Map */

#define PCIE_ARB_BASE_ADDR 0xE0000000

#define PCIE_ARB_END_ADDR 0xFFFFFFFF

But System crash happened in function imx_pcie_regions_setup.

I am curious about the fundamental question whether it is  possible to increase

PCIe memory by modifying or not? moreover, Can we assign memory resource to another place?

Best regards

Aden Yoon

0 项奖励
回复

1,902 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the recent BSP L.3.14.28

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

  In particular You may look at section 42.3 (System Resource: Memory Layout) of

“i.MX_6_Linux_Reference_Manual.pdf” regarding PCIe memory usage.

Total memory size is up to 16 MB.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,902 次查看
phanthavongdoua
NXP Employee
NXP Employee

Hi Yuri,

I have similar issue where my device driver failed to allocate memory for the bars and I am using 3.14.28

imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x1000-0x10000]

pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

pci_bus 0000:00: root bus resource [bus 00-ff]

pci_bus 0000:00: scanning bus

pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400

pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]

pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]

pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c

pci 0000:00:00.0: supports D1

pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold

pci 0000:00:00.0: PME# disabled

pci_bus 0000:00: fixups for bus

PCI: bus0: Fast back to back transfers disabled

pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0

pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1

pci_bus 0000:01: scanning bus

pci 0000:01:00.0: [1a33:8201] type 00 class 0x040000

pci 0000:01:00.0: reg 0x10: [mem 0xff000000-0xffffffff]

pci 0000:01:00.0: reg 0x20: [mem 0xffff0000-0xffffffff]

pci 0000:01:00.0: reg 0x24: [mem 0xfffff000-0xffffffff]

pci 0000:01:00.0: calling pci_fixup_ide_bases+0x0/0x3c

pci 0000:01:00.0: PME# supported from D0 D3hot

pci 0000:01:00.0: PME# disabled

pci_bus 0000:01: fixups for bus

PCI: bus1: Fast back to back transfers disabled

pci_bus 0000:01: bus scan returning with max=01

pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01

pci_bus 0000:00: bus scan returning with max=01

pci 0000:00:00.0: fixup irq: got 20

pci 0000:00:00.0: assigning IRQ 20

pci 0000:01:00.0: fixup irq: got 20

pci 0000:01:00.0: assigning IRQ 20

pci 0000:00:00.0: BAR 14: can't assign mem (size 0x1800000)

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

pci 0000:01:00.0: BAR 0: can't assign mem (size 0x1000000)

pci 0000:01:00.0: BAR 4: can't assign mem (size 0x10000)

pci 0000:01:00.0: BAR 5: can't assign mem (size 0x1000)

pci 0000:00:00.0: PCI bridge to [bus 01]

pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt

pci 0000:01:00.0: Signaling PME through PCIe PME interrupt

pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded

0 项奖励
回复

1,902 次查看
phanthavongdoua
NXP Employee
NXP Employee

Hi Yuri,

Here is the link for my discussion if you can help with:

Re: Adding PCI-e device driver for SABRE-SD board

Regards,

Phan. Douangphachanh

0 项奖励
回复