i.MX6ULZ pin description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULZ pin description

ソリューションへジャンプ
2,114件の閲覧回数
j_araya
Contributor II

Dear all,

I would like to ask whether there is a list with the pin description of the whole processor. We are developing a customized hardware with a PSRAM interface connected to the EIM port but the lack of a comprehensive pin description makes the pin matching with peripherals hard.

Can you give me any advice on that?

Thanks in advance!

Jose 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,900件の閲覧回数
pierre_lansac
Contributor I

Hello Jose,

You will find pins descriptions https://www.nxp.com/docs/en/data-sheet/IMX6ULZCEC.pdf 

see chapter : 4.9.3 External Interface Module (EIM)  

and chapter : 6 Package information and contact assignments

And more with the reference Manual https://www.nxp.com/webapp/Download?colCode=IMX6ULZRM 

Chapter 6  External Memory Controllers
Chapter 21 External Interface Module (EIM)

you also have Pins Tool for i.MX Application Processors | NXP but see Supported Devices ...

and look this extracted page from MCIMX6UL-EVKB

But I think you already read it all ... ...

BR

Pierre.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,901件の閲覧回数
pierre_lansac
Contributor I

Hello Jose,

You will find pins descriptions https://www.nxp.com/docs/en/data-sheet/IMX6ULZCEC.pdf 

see chapter : 4.9.3 External Interface Module (EIM)  

and chapter : 6 Package information and contact assignments

And more with the reference Manual https://www.nxp.com/webapp/Download?colCode=IMX6ULZRM 

Chapter 6  External Memory Controllers
Chapter 21 External Interface Module (EIM)

you also have Pins Tool for i.MX Application Processors | NXP but see Supported Devices ...

and look this extracted page from MCIMX6UL-EVKB

But I think you already read it all ... ...

BR

Pierre.

0 件の賞賛
返信