i.MX6ULZ pin description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULZ pin description

Jump to solution
2,069 Views
j_araya
Contributor II

Dear all,

I would like to ask whether there is a list with the pin description of the whole processor. We are developing a customized hardware with a PSRAM interface connected to the EIM port but the lack of a comprehensive pin description makes the pin matching with peripherals hard.

Can you give me any advice on that?

Thanks in advance!

Jose 

Labels (1)
0 Kudos
Reply
1 Solution
1,855 Views
pierre_lansac
Contributor I

Hello Jose,

You will find pins descriptions https://www.nxp.com/docs/en/data-sheet/IMX6ULZCEC.pdf 

see chapter : 4.9.3 External Interface Module (EIM)  

and chapter : 6 Package information and contact assignments

And more with the reference Manual https://www.nxp.com/webapp/Download?colCode=IMX6ULZRM 

Chapter 6  External Memory Controllers
Chapter 21 External Interface Module (EIM)

you also have Pins Tool for i.MX Application Processors | NXP but see Supported Devices ...

and look this extracted page from MCIMX6UL-EVKB

But I think you already read it all ... ...

BR

Pierre.

View solution in original post

0 Kudos
Reply
1 Reply
1,856 Views
pierre_lansac
Contributor I

Hello Jose,

You will find pins descriptions https://www.nxp.com/docs/en/data-sheet/IMX6ULZCEC.pdf 

see chapter : 4.9.3 External Interface Module (EIM)  

and chapter : 6 Package information and contact assignments

And more with the reference Manual https://www.nxp.com/webapp/Download?colCode=IMX6ULZRM 

Chapter 6  External Memory Controllers
Chapter 21 External Interface Module (EIM)

you also have Pins Tool for i.MX Application Processors | NXP but see Supported Devices ...

and look this extracted page from MCIMX6UL-EVKB

But I think you already read it all ... ...

BR

Pierre.

0 Kudos
Reply