i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

Jump to solution
1,033 Views
janezdolenc
Contributor I

Hello ,

I am starting HW design with i.MX6ULL. i.MX6ULL supports up to 2 Ethernet interfaces (ENET1 and ENET2), but I am using version with only 1 Ethernet (MCIMX6Y1CVM05AB ).

I couldn't find information in DS and RM which interface is active ENET1 or ENET2 ?

The same question could be for other interfaces (UART , I2C , USB , …).

It seems logical that first (or first 2 , or first 4) interface is active, it means ENET1 in my case, but I would like to get explicit information regarding this.

Regards ,

Janez Dolenc

Labels (1)
0 Kudos
Reply
1 Solution
1,028 Views
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,029 Views
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

0 Kudos
Reply