i.MX6ULL internal Flash jtag programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL internal Flash jtag programming

1,999件の閲覧回数
karsten
Contributor I

Hi,

at the moment I am starting with the i.MX6ULL at a custom board.

I use the document "Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives " to nice start.

Until now I was able to download and debug (Segger Base Debug Probe) the "Hello World"  example from SDK_2.2_MCIM6ULL .

I downloaded in the DDR and it works.

Now I would like to download and debug in the flash memory. Is this possible with an internal flash-memory of the i.MX6 or  is it necessary to have an external flash-memory ?

In  the memory map is a QSPI1 Memory, is this only for external connection or is this a real internal flash which i can use to program.

memory_map_iMX6ULL.PNG

Moreover I have an external NAND Flash. Is it possible to program this via Jtag and use it for my application ?

Best regards

Karsten

ラベル(1)
0 件の賞賛
返信
1 返信

1,782件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Karsten

for programming images to flash MFG Tool is used, this is described in

sect.5 Run a demo using Manufacturing Tool (MFGTool)

Getting Started with MCUXpresso SDK for i.MX 6ULL Derivatives

For nand one can look at

How-To use NAND boot on i.MX6UL EVK board 

Unfortunately I am not aware of options for programming flashes using jtag.

i.MX6ULL has not internal flash-memory.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信