i.MX6ULL framebuffer broken after resume from suspend

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL framebuffer broken after resume from suspend

507件の閲覧回数
tarjeiknapstad
Contributor II

On Yocto Scarthgap I am experiencing an issue with the framebuffer device not working after resuming from suspend. When resuming, the contents of the display from just before the suspend is displayed for a brief moment until the RUN bit is set in the LCD_CTRL register from the mxsfb.c device driver. This is an LCD screen in DOTCLOCK mode. This is with the linux 6.6 branch from linux-imx from the Yocto Scarthgap layers.

This used to work fine under mickledore, but now seems comlpetely broken. Any ideas what could be wrong?

0 件の賞賛
返信
1 返信

468件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

This created a bug in our system, developers will fix it ASAP. thanks for the catch!.

Regards

0 件の賞賛
返信