i.MX6ULL USB_OTG2 ROM loader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL USB_OTG2 ROM loader

Jump to solution
2,551 Views
chris321
Contributor IV

Hello,

according to the i.mx6ULL reference manual it is possible to use both USB OTG ports for ROM loading purposes.

Is the USB_OTG_ID pin analyzed by the ROM?

I want to use the USB_OTG2 port for manufacturing a custom board and after that it should be in host mode.

I plan to use the following pads for the muxable USB signals:

usb_otg2_id -->GPIO1_IO05

usb_otg2_oc --> SD1_DATA2

usb_otg2_pwr -->SD1_DATA1

I have a reference kit (compute module + base board) on my desk.

Is it possible to force the ROM loader to use the USB_OTG2 interface somehow?

Labels (2)
0 Kudos
Reply
1 Solution
2,388 Views
igorpadykov
NXP Employee
NXP Employee

Hi chris321

USB_OTG_ID pin is not analyzed by the ROM. Also only USB_OTG1

is used by ROM according to i.MX6ULL Reference Manual sect.8.2.4 Serial Downloader

https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,389 Views
igorpadykov
NXP Employee
NXP Employee

Hi chris321

USB_OTG_ID pin is not analyzed by the ROM. Also only USB_OTG1

is used by ROM according to i.MX6ULL Reference Manual sect.8.2.4 Serial Downloader

https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,388 Views
chris321
Contributor IV

Hi Igor, thank you for this answer.

According to the Reference Manual sect 8.9.1:

"The ROM supports the USB OTG port for boot purposes. The other USB ports on the chip are not supported for boot purposes."

I thought all the OTG ports are available for boot purposes.

0 Kudos
Reply