i.MX6ULL USB Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6ULL USB Configuration

1,688 次查看
ban45
Contributor III

Hi

Use i.MX6ULL as the device side instead of the USB host side.

Is it necessary to set the device tree? Is it necessary to set registers etc.?

Best regard.

0 项奖励
回复
3 回复数

1,682 次查看
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  Generally for USB specific devices, specific drivers should be used.
As for NXP Linux BSP, it supports in peripheral mode  MSC, and CDC
(Communication Devices Class) drivers, which include Ethernet and serial
support.

Regards,
Yuri.

0 项奖励
回复

1,652 次查看
ban45
Contributor III

Hi,

I bought an IC and made a prototype board instead of a commercially available development board.
Where should I get the USB driver?

best regard

0 项奖励
回复

1,646 次查看
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Use section 4.9 (USB) of "i.MX_Reference_Manual.pdf", in particular -
section 4.9.6 (Menu Configuration Options).

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards,
Yuri.

0 项奖励
回复