i.MX6ULL USB Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL USB Configuration

1,665 Views
ban45
Contributor III

Hi

Use i.MX6ULL as the device side instead of the USB host side.

Is it necessary to set the device tree? Is it necessary to set registers etc.?

Best regard.

0 Kudos
Reply
3 Replies

1,659 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

  Generally for USB specific devices, specific drivers should be used.
As for NXP Linux BSP, it supports in peripheral mode  MSC, and CDC
(Communication Devices Class) drivers, which include Ethernet and serial
support.

Regards,
Yuri.

0 Kudos
Reply

1,629 Views
ban45
Contributor III

Hi,

I bought an IC and made a prototype board instead of a commercially available development board.
Where should I get the USB driver?

best regard

0 Kudos
Reply

1,623 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Use section 4.9 (USB) of "i.MX_Reference_Manual.pdf", in particular -
section 4.9.6 (Menu Configuration Options).

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

 

Regards,
Yuri.

0 Kudos
Reply