i.MX6ULL UART(RTS CTS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL UART(RTS CTS)

3,136件の閲覧回数
ban45
Contributor III

Hi

I swapped only CTS and RTS using the CnfigTools for i.MX Version 9.0, but no error or warning. (TX, RX are unchanged)
Which register should be changed to switch the functions in use? Is it possible to replace CTS and RTS without changing TX and RX?

best regard

0 件の賞賛
返信
2 返答(返信)

3,129件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yasunori

 

>Is it possible to replace CTS and RTS without changing TX and RX?

 

sorry this is not possible. For details one can look at Figure 55-2. UART external signals

to module signals routing with respect to DCE/DTE mode

i.MX 6ULL Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信

3,126件の閲覧回数
ban45
Contributor III

Hi

Both can be set with the tool.
Do the RTS and CTS listed in the tool mean DCE / DTE = 0?

best regard

0 件の賞賛
返信