i.MX6ULL PXP using QT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL PXP using QT

3,742 Views
jimmyli
Contributor V

Hi,

    I found that i.mx6ull pxp can support image rotation, scaling, and so on.

    Now I will use QT4.8.4 to develop the project.

    I have a question: can QT4.8.4 apply pxp to accelerate image rotation, scaling, and so on?

    Thanks a lot.

Labels (2)
0 Kudos
Reply
2 Replies

3,288 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jimmy

yes pxp can be used to accelerate image rotation, scaling, however according to

p.10 attached Release Notes:

On SoCs without hardware graphics acceleration (GPU) for Frame Buffer, X11 or Wayland graphic backends
QT5 is handled only using mesa software graphics, and it is not supported by NXP.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,288 Views
jimmyli
Contributor V

Hi Igor,

    Thanks for your information.

0 Kudos
Reply