i.MX6ULL PXP using QT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL PXP using QT

3,746件の閲覧回数
jimmyli
Contributor V

Hi,

    I found that i.mx6ull pxp can support image rotation, scaling, and so on.

    Now I will use QT4.8.4 to develop the project.

    I have a question: can QT4.8.4 apply pxp to accelerate image rotation, scaling, and so on?

    Thanks a lot.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,292件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jimmy

yes pxp can be used to accelerate image rotation, scaling, however according to

p.10 attached Release Notes:

On SoCs without hardware graphics acceleration (GPU) for Frame Buffer, X11 or Wayland graphic backends
QT5 is handled only using mesa software graphics, and it is not supported by NXP.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,292件の閲覧回数
jimmyli
Contributor V

Hi Igor,

    Thanks for your information.

0 件の賞賛
返信