i.MX6ULL Linux Display Drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL Linux Display Drivers

1,674件の閲覧回数
khollar
NXP Employee
NXP Employee

My customer is trying to find which Linux display drivers are available, and also what LCD Digital Drivers are supported with any existing Linux drivers.

 

Ideally something similar to the Himax HX8238-D see attached, we would like to use in the 8bit data/ SPI control mode.

ラベル(4)
0 件の賞賛
返信
1 返信

1,302件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The default BSP Supports SEIKO WVGA panel. For i.MX 6UltraLite, i.MX 6ULL and i.MX 7Dual SABRE-SD, it supports Embest LCD8000-43T LCD panel.The LCD interface driver supports the Samsung LMS430xx 4.3" WQVGA LCD panel.

mxc_lcdif.c Display Driver for CLAA-WVGA and SEIKO-WVGA LCD support.Here if you want to use other LCD, you can connect and porting the screen driver to your board.

All the function and BSP Supported Features you can see the documents i.MX_Linux_Release_Notes.pdf and i.MX_Linux_Reference_Manual.pdf.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信