i.MX6UL u-boot doesn't recognize eMMC 5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL u-boot doesn't recognize eMMC 5.1

2,758 Views
renefed
Contributor I

Hi all,

on our custom board with i.MX6UL and eMMC 5.1, the bootloader doesn't recognize the eMMC.

The bootloader is loaded in serial download mode with the imx_usb_loader tool.

In uboot the following answers are shown:

mmc info => no card present

mmc dev 1 => Card did not respond to voltage select

The eMMC schematic is the same as in i.MX6UL EVK.

The u-boot is made with fsl-arm-yocto-bsp (mx6ul_14x14_evk).

Has u-boot to be modified working with eMMC 5.1? 

best regrads

René

Labels (3)
0 Kudos
Reply
1 Reply

2,055 Views
igorpadykov
NXP Employee
NXP Employee

Hi René

is emmc working in linux or freertos (for example booting from other media like sd):

Board Support Packages (7)
SDK2.2_iMX6UL_WIN(REV SDK2.2)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-processors/i.mx-6-pr...

one can check guidelines on

EMMC 5.0 and EMMC 5.1 work on i.MX6
https://community.nxp.com/docs/DOC-332187

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply