i.MX6UL Power-Rails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL Power-Rails

Jump to solution
1,992 Views
juergene
Contributor III

Hello community,

i wanted to know, why are the following power rails shown in the MCIMX6UL-EVK design schematic

VDD_ARM_IN: 400 mA

VDD_SOC_IN: 500 mA

pastedImage_1.png

Because there is only one power rail and this is VDD_SOC_IN.

Defined with a maximum supply current of 500 mA (i.MX6UL datasheet)

pastedImage_0.png

Does it mean the i.MX6UL need more than 500 mA at VDD_SOC_IN - Rail (900 mA given from schmeatic) ?

Best regards

Labels (1)
0 Kudos
Reply
1 Solution
1,858 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Juergen Elst,

The values on the i.MX6UL Datasheet are correct. I would say that the reason why there is more capacity on the schematic is because it’s using LDOs instead of a PMIC so they are listing the capacity of the LDO itself rather than the requirements.

The extra current does not hurt but should not be required.

Regards,

View solution in original post

1 Reply
1,859 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Juergen Elst,

The values on the i.MX6UL Datasheet are correct. I would say that the reason why there is more capacity on the schematic is because it’s using LDOs instead of a PMIC so they are listing the capacity of the LDO itself rather than the requirements.

The extra current does not hurt but should not be required.

Regards,