i.MX6UL ADC: VrefH input current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6UL ADC: VrefH input current

跳至解决方案
1,418 次查看
johannesdev
Contributor III

Hi!

We are designing an application with the i.MX6UL's internal ADC in use. An external shut voltage reference is connected to the SoC's VrefH input.

However, the datasheet of the i.MX6UL does not specify the input current on pin VrefH. Thus, I cannot calculate an appropriate bias current for the shunt reference. Is this value known?

Best regards,
Johannes

0 项奖励
回复
1 解答
1,361 次查看
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,362 次查看
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

0 项奖励
回复