i.MX6Sololite EVK Board Cannot Install Apps

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Sololite EVK Board Cannot Install Apps

1,579 次查看
nicholassaulnie
Contributor II

Hello All,

The Android 4.0.4 image that comes packaged with the EVK board can install APK files from the internet as long as I enable "unknown sources" under security settings and "usb debugging" under developer options.

I built a version of Android 4.0.4 loosely following the instructions in file 13.5.0_Android_User_Guide from IMX6_R13.5_ANDROID_DOCS_BUNDLE. The built Android seems to work; however, whenever I try to install a downloaded APK file it fails with on-screen message "Application not installed". No serial output is generated when the application fails to install.

Can anyone help me debug and fix this issue?

Thank you,

Nick

标签 (3)
0 项奖励
回复
2 回复数

1,479 次查看
nicholassaulnie
Contributor II

Is it possible that the system would generate an error when it failed to install the app? If so, where would I look to see this error?

0 项奖励
回复

1,479 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Nicholas,

Are you using ADB to install the APK?

0 项奖励
回复