i.MX6Solo:UART DMA transfer problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6Solo:UART DMA transfer problem

跳至解决方案
1,814 次查看
koichisakagami
Contributor II

Dear community,

We have been developing our product with iMX6Solo.

[Background]
When we use the UART DMA transfer with "RXTL=8 CTSTL=8", it works fine.
However, when we use the UART DMA transfer with "RXTL=16 CTSTL=16",unnecessary data are included in RX data.


The unnecessary data are not included in the real waveform.
The appearance frequency of unnecessary data is high-frequency.
The unnecessary data appear 8 byte order.

[Question]
We changed only " RXTL and CTSTL field".

Why are the unnecessary data included in RX data ?
Do we have to set any register other than RXTL and CTSTL  in order to work uart module correctly ?

We attached log file. (Red character is unnecessary data.)
Could you check it and advise us  ?

[   52.059266] [bt] open ttymxc1

[   52.059284] [bt] UCR1 = 0x00000021

[   52.059294] [bt] UCR2 = 0x00000007

[   52.059303] [bt] UCR3 = 0x00000784

[   52.059311] [bt] UCR4 = 0x00004000

[   52.059358] [bt] set ttymxc1 speed: 9600

[   52.059368] [bt] UCR1 = 0x00000d2d

[   52.059376] [bt] UCR2 = 0x00004027

[   52.059383] [bt] UCR3 = 0x00000784

[   52.059391] [bt] UCR4 = 0x00004040

[   52.059628] [bt] set ttymxc1 speed: 9600

[   52.059641] [bt] UCR1 = 0x00000d2d

[   52.059650] [bt] UCR2 = 0x00002027

[   52.059658] [bt] UCR3 = 0x00000784

[   52.059665] [bt] UCR4 = 0x00004040

[   52.059721] [bt] set ttymxc1 speed: 115200

[   52.059731] [bt] UCR1 = 0x00000d2d

[   52.059739] [bt] UCR2 = 0x00002027

[   52.059746] [bt] UCR3 = 0x00000784

[   52.059754] [bt] UCR4 = 0x00004040

[   52.237021] [bt] USR1 = 0x00006040

[   52.237031] [bt] USR2 = 0x00004008

[   52.237043] [bt] rx: 04 0E 04 04 03 0C 00

[   52.237049] [bt] USR1 = 0x00006040

[   52.237053] [bt] USR2 = 0x00004008

[   52.268972] [bt] rx: 04 0E 0B 04 05 10 00 FD 00 00 00 00 00 00 00 00 03 FE 04 00

[   52.268980] [bt] rx: 03 00

[   52.268988] [bt] USR1 = 0x00006040

[   52.268992] [bt] USR2 = 0x00004008

[   52.309350] [bt] rx: 04 0E 04 04 33 0C 01

[   52.309370] [bt] USR1 = 0x00006040

[   52.309379] [bt] USR2 = 0x00004008

[   52.338923] [bt] rx: 04 0E 0C 04 03 10 00 FF 03 03 03 03 03 03 03 03 FB AD FE DB

[   52.338933] [bt] rx: FF 7B 87

[   52.338942] [bt] USR1 = 0x00006040

[   52.338946] [bt] USR2 = 0x00004008

[   52.368318] [bt] rx: 04 0E 0E 04 04 10 00 01 03 03 03 03 03 03 03 03 01 00 00 00

[   52.368328] [bt] rx: 00 00 00 00 01 01 01 01 01 01 01 01 00

[   52.368336] [bt] USR1 = 0x00006040

[   52.368340] [bt] USR2 = 0x00004008

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,689 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

In general this may be caused by fact that sdma script watermark level

also should be changed when RXTL changed. Please note that

FSL provides BSPs with thoroughly tested sdma scripts and

drivers which use these scripts.  Sorry, FSL does not support

modifications and customizations sdma scripts and drivers using them.

If you have special reasons for that please elevate this through local marketing.

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,690 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Koichi

In general this may be caused by fact that sdma script watermark level

also should be changed when RXTL changed. Please note that

FSL provides BSPs with thoroughly tested sdma scripts and

drivers which use these scripts.  Sorry, FSL does not support

modifications and customizations sdma scripts and drivers using them.

If you have special reasons for that please elevate this through local marketing.

Best regards

igor

0 项奖励
回复
1,689 次查看
koichisakagami
Contributor II

Dear Igor san,

Thank you for your advice.

We will check them.

Best regards

Sakagami

0 项奖励
回复