Hi Igor,
I understood the hardware supported format.
Then, I want to know the software supported format by BSP also.
I checked Linux reference manual of some revision (L3.0.35, L3.10.17, L3.10.53, and L3.14.28), and there is no description about 24 bits audio in these reference manual even though there is the description about 16 bits audio.
And in source codes (imx-hdmi-dma.c) of these revision, 24 bits audio seems to be not supported.
So I believe 24 bits format by software, is this correct?
Best Regards,
Satoshi Shimoda