i.MX6SDL GPIO current.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL GPIO current.

Jump to solution
1,915 Views
takashitakahash
Contributor III

Hi community.

Our customer has tree question below.Would please advice.

Q1,

The absolute maximum rating of the output current of the GPIO?

Is to destroy and too much current through CMOS transistors?

Q2,

My understanding is correct ? The output current is limited by the VOH/VOL and the DSE.

The examples listed below.

Design examples)OVDD=3.3V and DSE:111 = 20 Ω than (Table36 of IMX6SDLAEC ), VOH=2.64V, VOL=0.66V design.

Ioh = (OVDD-VOH) / 20 Ω = (3.3-2.64) / 20 = 33 mA

IOL = Ω = 0.66 VOL 20 / 20 = 33 mA

Therefore, less than 33 mA output current in order to satisfy the VOH/VOL.

Q3,

For our specific use cases.

May be used currently in our system GPIO ports up to 1.3 mA (only one port. Others are used in less than 1 mA).

At this time, the VOH output of 3.3 V. But we would not be able to destroy ?.

Labels (2)
0 Kudos
Reply
1 Solution
1,757 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. absolute maximum rating of the output current of the GPIO

is not specified by datasheet, yes it is limited by allowable temperature,

which is defined.

2. if you have VOH=2.64V, VOL=0.66V in design, then I believe

this understanding is correct

3. GPIO ports up to 1.3 mA can be used. Regarding "At this time, the VOH output of 3.3 V"

seems datasheet has not such parameter. Please check Table 23. GPIO DC Parameters

i.MX6SDL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,758 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

1. absolute maximum rating of the output current of the GPIO

is not specified by datasheet, yes it is limited by allowable temperature,

which is defined.

2. if you have VOH=2.64V, VOL=0.66V in design, then I believe

this understanding is correct

3. GPIO ports up to 1.3 mA can be used. Regarding "At this time, the VOH output of 3.3 V"

seems datasheet has not such parameter. Please check Table 23. GPIO DC Parameters

i.MX6SDL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply