i.MX6S USB_H1_VBUS pin when power off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S USB_H1_VBUS pin when power off

Jump to solution
2,763 Views
torus1000
Contributor V

Hi,

I want to confirm about VBUS pin as following.

According to the i.MX6S/DL datasheet, USB_H1_VBUS input pin seems separated from other power domains.

NOTE
USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.


4.3.2.3 LDO_USB
The LDO_USB module implements a programmable linear-regulator function from the
USB_OTG_VBUS and USB_H1_VBUS voltages (4.4 V–5.25 V) to produce a nominal 3.0 V output voltage.

Is it OK to leave USB_H1_VBUS supplying 5V for a while even all other power supply were off?

Can anyone help?

Labels (1)
0 Kudos
Reply
1 Solution
2,573 Views
igorpadykov
NXP Employee
NXP Employee

Hi  torus1000

yes acceptable.

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
2,573 Views
torus1000
Contributor V

Dear Igor igorpadykov

Just in case,

Is it acceptable to keep same situation(all powers off except USB 5V) over 72 hours?

Thanks

0 Kudos
Reply
2,574 Views
igorpadykov
NXP Employee
NXP Employee

Hi  torus1000

yes acceptable.

Best regards
igor

0 Kudos
Reply
2,573 Views
igorpadykov
NXP Employee
NXP Employee

Hi  torus1000

>Is it OK to leave USB_H1_VBUS supplying 5V for a while even all other power supply were off?

yes it is OK.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------