Hi community,
I have a question about i.MX6S CLKO.
I tried output 32kHz from CCM_CLKO1 with the following settings.
However, it does not output even though external 32kHz crystal oscillates certainly.
=====
IOMUXC_SW_MUX_CTL_PAD_GPIO05 = 3; (Select CCM_CLKO1, SION=0)
IOMUXC_SW_PAD_CTL_PAD_GPIO05 = 0x0001B0B0;
CCM Clock Output Source Register (CCM_CCOSR)
8 CLK_OUT_SEL : 0 CCM_CLKO1 output drives CCM_CLKO1 clock
7 CLKO1_EN : 1 CCM_CLKO1 enabled.
6-4 CLKO1_DIV : 000 divide by 1(default)
3-0 CLKO1_SEL : 1110 ckil_sync_clk_root
=====
[Q]
Is any additional setting needed to output 32kHz from CCM_CLKO1?
If no additional setting is needed, could you let me know what is considered as a possibility of a root cause?
For your information, 24MHz is output from CCM_CLKO2 with similar setting as above.
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
I just tried it on i.MX6DL sabresd board, and CLKO1 can output 32KHz clock. Below is the config
r159 on i.MX6DL SabreSD board, pin GPIO_0
0x20e020c set to 0 to select it as CLKO1;
0x20e05dc set to 0x1b0b0;
0x20c4060 set to 0x8e to select ckil sync clock output.
Then there will be 32KHz clock output on r159.
I also tried GPIO_5 pin, set 0x20e0230 to 3, we can see 32KHz clock on r66 of i.MX6DL SabreSD board.
Hi Yuri, Yongcai,
Thank you for your cooperation.
I got a report from measurement member about root cause.
It was a board pattern issue, the pattern was cut by high temperature.
So now, 32kHz is output correctly from CLKO1 on other board that has no pattern issue.
I appreciate your great support!
Can anyone reply me?
Is CLKO 32 KHz output just a DC level or some waveforms (which look as some kind of noise) may be observed ?
Hi Yuri,
I'm checking it to measurement member.
Just a moment please?
Best Regards,
Satoshi Shimoda
I just tried it on i.MX6DL sabresd board, and CLKO1 can output 32KHz clock. Below is the config
r159 on i.MX6DL SabreSD board, pin GPIO_0
0x20e020c set to 0 to select it as CLKO1;
0x20e05dc set to 0x1b0b0;
0x20c4060 set to 0x8e to select ckil sync clock output.
Then there will be 32KHz clock output on r159.
I also tried GPIO_5 pin, set 0x20e0230 to 3, we can see 32KHz clock on r66 of i.MX6DL SabreSD board.