i.MX6Quad RTC typical power consumption in SNVS mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Quad RTC typical power consumption in SNVS mode

Jump to solution
2,265 Views
RussellPead
Contributor II
  1. For the i.MX6Quad, is the 4uA typical for an external crystal for the RTC (Table 19 page 35) included in the 41uA typical in SNVS mode (Table 9 page 25) or is it separate with total current 45uA typical?


Referenced Document Number: IMX6DQIEC     i.MX6D/Q Datasheet

Rev. 3, 03/2014

0 Kudos
Reply
1 Solution
1,973 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,974 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,973 Views
igorpadykov
NXP Employee
NXP Employee

Hi Russell

yes this data is included in 41uA typical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply