i.MX6Q UART SDMA issue on ARM2 -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q UART SDMA issue on ARM2 -blog archive

5,325 Views
ethan_cheng
NXP Employee
NXP Employee

There are two uart which are ttymxc1 and ttymxc3 on ARM2, and usually ttymcx3 is used for console.
If we use ttymxc1 to transmit data from PC to ARM2, it will get an error message "We cannot prepare for the RX slave dma!" and the transmission will be stopped randomly.
The root cause of this issue is software process of SDMA could be mistaken when an unexpected hardware interrupt was happened.
Let have a look about SDMA source code.

static int sdma_run_channel(struct sdma_channel *sdmac)
{
 struct sdma_engine *sdma = sdmac->sdma;
 int channel = sdmac->channel;
 int ret;

 init_completion(&sdmac->done);

 wmb();
 __raw_writel(1 << channel, sdma->regs + SDMA_H_START);  // (1) Start SDMA channel to load script.

 ret = wait_for_completion_timeout(&sdmac->done, HZ);  // (2) Wait for SDMA interrupt to indicate script loading is completed.

 return ret ? 0 : -ETIMEDOUT;
}

static void mxc_sdma_handle_channel(struct sdma_channel *sdmac)
{
 complete(&sdmac->done);  // (3) Inform script loading is completed.

 /* not interested in channel 0 interrupts */
 if (sdmac->channel == 0)
  return;

 if (sdmac->flags & IMX_DMA_SG_LOOP)
  sdma_handle_channel_loop(sdmac);
 else
  mxc_sdma_handle_channel_normal(sdmac);
}

The correct process we expected is (1) -> (2) -> (3).
But, a bug exists in this software design when an unexcepted hardware interrupt was happened between (1) and (2).

Please think about the below scenario.
 __raw_writel(1 << channel, sdma->regs + SDMA_H_START);  // (1) Start SDMA channel to load script
 other hardware interrupt ISR;
 SDMA hardware interrupt ISR;  // (3) will be executed.
 ret = wait_for_completion_timeout(&sdmac->done, HZ);  // (2) Wait for SDMA interrupt to indicate script loading is completed.

The process flow will be (1) -> (3) -> (2) and it causes (2) to get timeout and return an error code.
Solution A:
Use a work queque to execute "complete" function in SDMA interrupt handler.
The drawback is the performance of SDMA will be affected.

Solution B:
Re-load the script/context when receiving (2) timeout error code.
Because this bug as the above described is happened seldom, this solution should be acceptable.

Tags (1)
9 Replies

3,372 Views
keitanagashima
Senior Contributor I

Hi Cheng,

My customer is encountering this error, while communicating to a bluetooth module.

Is it supporting the UART SDMA issue in L3.14.28_1.0.0?

Best Regards,

Keita

0 Kudos
Reply

3,372 Views
sbergsma
Contributor I

Hi Cheng,

We use Freescale i.MX6Q with Linux 3.0.35_4.0.0

We use ttymxc2 @ 115k2 without RTS/CTS

We use ttymxc0 for @ 115k2 without RTS/CTS for communication with our machine.

When i do put a linux console on ttymxc2 sometimes suddenly it stops working and then i get:

"We cannot prepare for the RX slave dma!"

So it looks that the issue you described is not fixed in 3.0.35_4.0.0 yet?

Is it fixed in 3.0.35_4.1.0?

Looking forward to your reply.

Sake

0 Kudos
Reply

3,372 Views
dmitriybeykun
Contributor I

I am also interested in fix for this issue, and I can tell that this is not fixed in the latest BSP releases.

I have a board that has bluetooth connected to UART with RTS/CTS which works okay *only if SDMA is disabled*. More info here Google Groups (last part of the post).

Hope to see answer from Freescale guys.

Best Regards,

Dmitriy Beykun

0 Kudos
Reply

3,372 Views
jiadawang
Contributor IV

Hi, Cheng

does UART SDMA must work with hardware flow control?

0 Kudos
Reply

3,372 Views
FrankLi1z
NXP Employee
NXP Employee

Yes. UART DMA need hardware flow control.

Best regards

Frank Li

0 Kudos
Reply

3,372 Views
jiadawang
Contributor IV

Hi, Zhi, li thank you for your confirm

I found in the UART DMA support patch

it also mentions DTE mode, does it mean UART SDMA also have to work in DTE mode?

0 Kudos
Reply

3,372 Views
Balaji_ng
Contributor III

Hi,

jiadawang wrote:

I found in the UART DMA support patch

    I am encountering this error, while communicating to a bluetooth module.Can you post the link to that patch?

Regards,

Balaji

0 Kudos
Reply

3,372 Views
speer
Contributor I

Very good sharing, thanks!

0 Kudos
Reply