i.MX6Q RWS_EN for Bayer/Raw image capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q RWS_EN for Bayer/Raw image capture

ソリューションへジャンプ
1,194件の閲覧回数
davemcmordie
Contributor III

Section 37.5.142 of the Reference Manual (IPUx_IC_CONF) refers to RWS_EN (Raw Sensor Enable).  It looks like this and CSI_MEM_WR_EN need to be set correctly to enable raw/Bayer/Monochrome sensors.  Yet I don't see this setting being set in the CSI_MEM case in the enable tasks method of ipu_ic.  Is this setting necessary to enable raw image capture, or is there another way to do it?

ラベル(3)
0 件の賞賛
返信
1 解決策
763件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
764件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

0 件の賞賛
返信