i.MX6Q NAND Flash in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q NAND Flash in Linux

4,081 Views
mahi
Contributor IV

Hi Community,

I have problems bringing up our custom board with NAND Flash using release-bsp 4.1.15-2.0.0.

In u-boot, I can access the flash without issues, so I think board and assembly are OK. In Linux, the NAND device is detected, but as soon as I try to access it in any way, I get the lollowing Error:

gpmi-nand 112000.gpmi-nand: DMA timeout, last DMA :2
gpmi-nand 112000.gpmi-nand: Show GPMI registers :
gpmi-nand 112000.gpmi-nand: offset 0x000 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x010 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x020 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x030 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x040 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x050 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x060 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x070 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x080 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x090 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x0a0 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x0b0 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x0c0 : 0xffffffff
gpmi-nand 112000.gpmi-nand: offset 0x0d0 : 0xffffffff
gpmi-nand 112000.gpmi-nand: Show BCH registers :
gpmi-nand 112000.gpmi-nand: offset 0x000 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x010 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x020 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x030 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x040 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x050 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x060 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x070 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x080 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x090 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0a0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0b0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0c0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0d0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0e0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x0f0 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x100 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x110 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x120 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x130 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x140 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x150 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x160 : 0x00000000
gpmi-nand 112000.gpmi-nand: offset 0x170 : 0x00000000
gpmi-nand 112000.gpmi-nand: BCH Geometry :
GF length              : 13
ECC Strength           : 8
Page Size in Bytes     : 2110
Metadata Size in Bytes : 10
ECC Chunk0 Size in Bytes: 512
ECC Chunkn Size in Bytes: 512
ECC Chunk Count        : 4
Payload Size in Bytes  : 2048
Auxiliary Size in Bytes: 16
Auxiliary Status Offset: 12
Block Mark Byte Offset : 1999
Block Mark Bit Offset  : 0
gpmi-nand 112000.gpmi-nand: Chip: 0, Error -110
libmtd: error!: MEMERASE64 ioctl gpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
failed for eraseblock 0 (mtd0)
 gpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
       error 5 (Input/output errogpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
r)
flash_erase: error!: /dev/mtdgpmi-nand 112000.gpmi-nand: Chip: 0, Error -22
0: MTD Erase failure

Kernel-Logs:

nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xaa
nand: Micron MT29F2G08ABBGAH4
nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128
Scanning device for bad blocks
1 cmdlinepart partitions found on MTD device gpmi-nand
Creating 1 MTD partitions on "gpmi-nand":
0x000000000000-0x000010000000 : "nand"
gpmi-nand 112000.gpmi-nand: driver registered.

mtdinfo:

bash-4.3# mtdinfo -a
Count of MTD devices:           1
Present MTD devices:            mtd0
Sysfs interface supported:      yes

mtd0
Name:                           nand
Type:                           nand
Eraseblock size:                131072 bytes, 128.0 KiB
Amount of eraseblocks:          2048 (268435456 bytes, 256.0 MiB)
Minimum input/output unit size: 2048 bytes
Sub-page size:                  2048 bytes
OOB size:                       128 bytes
Character device major/minor:   90:0
Bad blocks are allowed:         true
Device is writable:             true

Device Tree:

#include "imx6q.dtsi"

...

&iomuxc {

        pinctrl_gpmi: gmpigrp {
            fsl,pins = <
                MX6QDL_PAD_NANDF_ALE__NAND_ALE             0x0000B0B1
                MX6QDL_PAD_NANDF_CLE__NAND_CLE             0x0000B0B1
                MX6QDL_PAD_NANDF_CS0__NAND_CE0_B           0x0000B0B1
                MX6QDL_PAD_NANDF_D0__NAND_DATA00           0x0000B0B1
                MX6QDL_PAD_NANDF_D1__NAND_DATA01           0x0000B0B1
                MX6QDL_PAD_NANDF_D2__NAND_DATA02           0x0000B0B1
                MX6QDL_PAD_NANDF_D3__NAND_DATA03           0x0000B0B1
                MX6QDL_PAD_NANDF_D4__NAND_DATA04           0x0000B0B1
                MX6QDL_PAD_NANDF_D5__NAND_DATA05           0x0000B0B1
                MX6QDL_PAD_NANDF_D6__NAND_DATA06           0x0000B0B1
                MX6QDL_PAD_NANDF_D7__NAND_DATA07           0x0000B0B1
                MX6QDL_PAD_NANDF_RB0__NAND_READY_B         0x0000B000
                MX6QDL_PAD_NANDF_WP_B__NAND_WP_B           0x0000B0B1
                MX6QDL_PAD_SD4_CLK__NAND_WE_B              0x0000B0B1
                MX6QDL_PAD_SD4_CMD__NAND_RE_B              0x0000B0B1
                MX6QDL_PAD_SD4_DAT0__NAND_DQS              0x000000B1
            >;
        };

...

};

&gpmi {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_gpmi>;
   status = "okay";
};

Any ideas, what could be wrong?

Labels (2)
0 Kudos
Reply
2 Replies

2,800 Views
mahi
Contributor IV

I added

   nand-on-flash-bbt;
   fsl,use-minimum-ecc;

to the gpmi node in the device tree and now it seems to work.

Initially I only added "nand-on-flash-bbt", then the kernel stopped when trying to write a bad-block table.

0 Kudos
Reply

2,800 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

one can check nand kernel boot parameters described in Table 10. Common

kernel boot parameters attached Release Notes, example dts with nand:

imx6qdl-sabreauto.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply