i.MX6Q Encoder slice mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q Encoder slice mode

ソリューションへジャンプ
3,493件の閲覧回数
jotes
Contributor IV

Hi!

While encoding h.264 video in slice mode, how will I now, when a single slice is ready (for example to further processing)? As I understand vpu_IsBusy() and vpu_WaitForInt() are useful only when I want to encode frame by frame (not slice by slice).

Thanks!


ラベル(3)
0 件の賞賛
返信
1 解決策
2,933件の閲覧回数
eaglezhou
NXP Employee
NXP Employee

Hi,

  

     Only "frame by frame" output is supported by vpu, "slice by slice" output not supported,

     Slice mode means user can config vpu to encode multi-slice per frame, not means "slice by slice" output.

Regard

Eagle.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,934件の閲覧回数
eaglezhou
NXP Employee
NXP Employee

Hi,

  

     Only "frame by frame" output is supported by vpu, "slice by slice" output not supported,

     Slice mode means user can config vpu to encode multi-slice per frame, not means "slice by slice" output.

Regard

Eagle.

0 件の賞賛
返信
2,933件の閲覧回数
jotes
Contributor IV

Hi Peng Zhou,

I have another question in this topic.

Encoder can send the encoded bits after each slice. Can decoder start decoding after receiving one single slice? Or maybe it has to wait for whole complete frame?

Thanks!

0 件の賞賛
返信
2,933件の閲覧回数
eaglezhou
NXP Employee
NXP Employee

Hi, Jotes

  For iMX6 vpu decoder, there are two mode, rollback mode(vpu wait the whole frame ready), and interrupt mode(not required the whole frame ready)

  in rollback mode, user need to feed enough data to vpu, otherwise, vpu will return and report data isn't enough

  while in interrupt mode, vpu won't reuturn when the data isn't enough, and will enter busy state in which it will wait the following data.

  but for the output, only interrupt in frame level is sendout by vpu decoder for both mode,

Regard

Eagle

0 件の賞賛
返信
2,933件の閲覧回数
jotes
Contributor IV

So, to sum up:

  1. I can encode slice by slice and send one frame in few parts to decoder.
  2. In rollback mode I can't start decoding until I have a whole frame in decoder. When same parts of frame are missing, I can see the following warning: "vpu needs more bitstream in rollback mode".
  3. In interrupt mode I can start decoding even if only a part of frame (few slices) is received, but the output is generated after decoding whole frame.
  4. No matter if decoder works in interrupt mode or rollback mode, output is generated in the same time (after decoding the entire frame).

Is that correct?

0 件の賞賛
返信
2,933件の閲覧回数
eaglezhou
NXP Employee
NXP Employee

Hi, Jotes

    Your understanding are basically right.

    For 1, the output from encoder still is frame level.

Regard

Eagle.

0 件の賞賛
返信