i.MX6Q/EEPROM Recovery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q/EEPROM Recovery

ソリューションへジャンプ
2,266件の閲覧回数
soichiyamamoto
Contributor V

Hi,

There is EEPROM Recovery Enable in 8.5.5.1 Serial ROM eFUSE Configuration of i.MX 6Dual/6Quad Applications Processor Reference Manual.

Is this flag a function to perform what concretely?

Best Regards,

soichi

ラベル(2)
0 件の賞賛
返信
1 解決策
1,992件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

From section 8.9 (Recovery Devices) of the RM :

"The Chip supports recovery devices. If primary boot device fails, boot ROM will try to

boot from recovery device using one of I2C or ECSPI ports.

For enabling recovery device BOOT_CFG4[6] fuse must be set. Additionally Serial

EEPROM fuses must be set as described in Serial ROM through SPI and I2C."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,993件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

From section 8.9 (Recovery Devices) of the RM :

"The Chip supports recovery devices. If primary boot device fails, boot ROM will try to

boot from recovery device using one of I2C or ECSPI ports.

For enabling recovery device BOOT_CFG4[6] fuse must be set. Additionally Serial

EEPROM fuses must be set as described in Serial ROM through SPI and I2C."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信