Dears,
We'd like to design a customized board which support 4GB DDR3 RAM.
We had ever found Linux BSP 4.1.0, but it seems only 1GB and 2GB DDR3 codes we can refer .
Is there any reference Freescale evaluation boards in Linux BSP 4.1.0 or Yocto project we can reference? ex: we refer sabre-lite codes to develop 2GB DDR3 bsp.
Any ideas we can start to do if there is no 4GB DDR3 reference codes?
Thanks a lot.
解決済! 解決策の投稿を見る。
Hi Ezero
please look at attached 4GB script.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chipexpert,
For example:
[uboot]
dram_init()
{
...
gd->bd->bi_dram[0].size =.............;
}
[kernel]
./arch/arm/mach-mx6/board-mx6q_sabresd.c
mx6q_sabresd_reserve() {
...
phys = memblock_alloc_base(imx6q_gpu_pdata.reserved_mem_size, SZ_4K, 4u * 1024 * 1024 * 1024);
...
}
Thanks a lot.
chipexpert 留言:
Hi Ezero
please look at attached 4GB script.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ezero
4GB vs 2GB DDR3 codes changes are minimal, you can compare
settings in flash_header.S.
For memory (and other changes) one can look at
i.MX_6Dual6Quad_BSP_Porting_Guide.pdf
In uboot this will be in uboot/include/configs/board_xx.h.
Linux will see max. 3840MB as shown on sect.2.3 "DDR mapping to
MMDC controller ports" IMX6DQRM
Best regards
chip
Hi Chip,
Which flash_header.S can I compare? As I known "mx6q_arm2/flash_header.S", "mx6q_hdmidongle/flash_header.S" and "mx6q_sabreauto/flash_header.S" are 2GB settings. But I can't find similar 4GB RAM settings in u-boot.
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6sl_arm2/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6q_sabreauto/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6q_hdmidongle/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6q_sabresd/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6q_arm2/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6q_sabrelite/flash_header.S
./rpm/BUILD/u-boot-2009.08/board/freescale/mx6sl_evk/flash_header.S
Thanks.
chipexpert 留言:
Hi Ezero
4GB vs 2GB DDR3 codes changes are minimal, you can compare
settings in flash_header.S.
For memory (and other changes) one can look at
i.MX_6Dual6Quad_BSP_Porting_Guide.pdf
In uboot this will be in uboot/include/configs/board_xx.h.
Linux will see max. 3840MB as shown on sect.2.3 "DDR mapping to
MMDC controller ports" IMX6DQRM
Best regards
chip
Hi Ezero
I meant flash_header.S which you found with file which I sent.
Best regards
chip
Hi Chip,
I saw a file "MX61Q_4GB.inc.zip" in your reply on AUG/31. And I could connect to the links "L3.0.35_4.1.0_LINUX_DOCS" and " IMX6DQRM" replied by you on SEP 2.
But, I didn't see flash_header.S you sent.
I lost reply from you?
Thanks a lot.
Hi Ezero
I did not send flash_header.S.
I attached MX61Q_4GB.inc.zip" only
and suggest you to compare them (preferably with"mx6q_arm2/flash_header.S"
though it is not important) yourself.
Best regards
chip
Dear Chip,
Unfortunately, we got error when we try to use DDR stress tester on 4GB ram board.
Here is the log:
DDR stress tester v1.0.2 with i.MX6Q error
Total memory is 4G bytes, 8G bits Dual Die (2CS) * 4.
Detail log as attachments.
------------------------------------------------------------------
Would you like to run the write leveling calibration? (y/n)
Please enter the MR1 value on the initilization script
This will be re-programmed into MR1 after write leveling calibration
Enter as a 4-digit HEX value, example 0004, then hit enter
0000 You have entered: 0x0000
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x000D000B
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x0012000D
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00040012
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x017E000F
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
------------------------------------------------------------------
Would you like to run the write leveling calibration? (y/n)
Please enter the MR1 value on the initilization script
This will be re-programmed into MR1 after write leveling calibration
Enter as a 4-digit HEX value, example 0004, then hit enter
0004 You have entered: 0x0004
Start write leveling calibration
Write leveling calibration completed
MMDC_MPWLDECTRL0 ch0 after write level cal: 0x000E0006
MMDC_MPWLDECTRL1 ch0 after write level cal: 0x00150010
MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00040016
MMDC_MPWLDECTRL1 ch1 after write level cal: 0x017F000F
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
Could you please help us to review our script aid?
Thanks a lot.
BRs,
Ezero
Hi Ezero,
Before I use 4G bits (1CS) *4,total memory is 2G bytes is ok for me.
Now my board total memory is 4G bytes, 4G bits (2CS) *8.
I have met the same problem with you.
Have you solve your issues?
Could you give me some advices?
Thanks,
Leo
Hi Ezero
I would suggest to check carefully below link document,
in script for example tFAW is incorrect (should be 0x1F, if you read
attached datasheet https://community.freescale.com/servlet/JiveServlet/download/438061-281103/99H02-11185D.pdf
p.17, tFAW=32nCK for 2KB page)
"0xB8BE7955 // MMDC0_MDCFG0"
MX6 DRAM Port Application Guide-DDR3 link
https://community.freescale.com/docs/DOC-101708
However even with wrong values it is strange that it:
"dram test fails for all values."
This may point that smth severely wrong with hardware:
broken/missed/interchanged data/address lines e.t.c.
You can just run SDK simple ram test with jtag, testing signals
with oscilloscope. With low frequencies (about 200MHz) it should run
fine with reference board settings (*.inc files in tools/rvd folder).
Best regards
igor
Dear Chip,
Sorry for my misunderstanding.
BRs,
Ezero