i.MX6Q Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q Boot

1,412 次查看
vishakh
Contributor III

Hi,

We have custom developed i.MX6Q based SOM. In this we are observing following behaviour in boot media selection:

  1. Boot pins are set to mSD and mSD is not inserted, then Boot loader will boot from SPI-NOR Flash.
  2. Boot pins are set to mSD and mSD is present, Boot loader will boot from mSD.

Is this the expected behaviour, to boot from SPI-NOR flash if the selected boot media is not present?

Below is the i.MX6Q processor part number we are using:

MCIMX6Q5EYM12AD

With Regards,

Vishakh

0 项奖励
回复
1 回复

1,327 次查看
art
NXP Employee
NXP Employee

No, this is not the expected behaviour.

Best Regards,

Artur

0 项奖励
回复