i.MX6Q Boot

cancel
Showing results for 
Search instead for 
Did you mean: 

i.MX6Q Boot

121 Views
vishakh
Contributor III

Hi,

We have custom developed i.MX6Q based SOM. In this we are observing following behaviour in boot media selection:

  1. Boot pins are set to mSD and mSD is not inserted, then Boot loader will boot from SPI-NOR Flash.
  2. Boot pins are set to mSD and mSD is present, Boot loader will boot from mSD.

Is this the expected behaviour, to boot from SPI-NOR flash if the selected boot media is not present?

Below is the i.MX6Q processor part number we are using:

MCIMX6Q5EYM12AD

With Regards,

Vishakh

0 Kudos
1 Reply

36 Views
art
NXP TechSupport
NXP TechSupport

No, this is not the expected behaviour.

Best Regards,

Artur

0 Kudos