i.MX6DQ audio interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DQ audio interface.

跳至解决方案
802 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ audio interface.
Actually, our customer have used 3 audio inputs/outputs with SSI1 to SSI3.
In this case, can they add a new audio input/output with ESAI?

Would you let me know what is the maximum number of audio interface (SSI + ESAI) i.MX6DQ can be used?


Best Regards,
Satoshi Shimoda

标签 (4)
标记 (3)
0 项奖励
回复
1 解答
659 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
660 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

SSI and ESAI work independently from each other an may be used

together. There are no restricitions on number of audio interfaces (SSI + ESAI).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复