i.MX6DQ GPU stops.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,334件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner met a GPU problem with the following log on a i.MX6DQ android_jb4.2.2_1.1.0-ga based custom board..

<4>[galcore]: Can't dump when GPU is power off or clock off.

Would you let me know the condition to output the above log?

Only when GPU power or clock is gating as indicated the log?

Or is it output when GPU is hang up also?

Best Regards,

Satoshi Shimoda

タグ(1)
0 件の賞賛
返信
1 解決策
4,884件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please apply ENGR00322672 [#1244] avoid system freeze when dump GPU state without valid clock & power

described in attached document and link below

ARM / qmx6_kernel | GitLab

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,885件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please apply ENGR00322672 [#1244] avoid system freeze when dump GPU state without valid clock & power

described in attached document and link below

ARM / qmx6_kernel | GitLab

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,884件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

Thank you for your reply.

I think the patch is for L3.10.17_1.0.0-ga or later.

Then, I found same code in android_jb4.2.2_1.1.0-ga (kernel = L3.0.35_4.1.0) as below.

SBO069~B.PNG

So the following codes should be inserted after line 5727 in this case.

   gckOS_Delay(gcvNULL, gcdPOWEROFF_TIMEOUT);

   if (Hardware->chipPowerState != gcvPOWER_ON

    && Hardware->chipPowerState != gcvPOWER_IDLE

   )

   {

       gcmkPRINT("[galcore]: Can't dump when GPU is power off or clock off.");

       gcmkFOOTER_NO();

       return gcvSTATUS_OK;

   }

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信