imx6 as a USB charger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 as a USB charger

836 Views
宗標廖
Contributor V

Hello community

I want to know whether the i.MX6 device can be used as a USB charger to

charge usb device that connected to i.MX6.

There are descriptions in i.MX_6_Linux_Reference_Manual as bellow,what

does it mean?

-------------------------------------------------------------------------------------------------

41.2.9 USB Charger Detection

i.MX SoC has USB charger detection ability, but it has no charging ability.

-------------------------------------------------------------------------------------------------

Best Regards

ZongbiaoLiao

Labels (2)
0 Kudos
Reply
4 Replies

609 Views
igorpadykov
NXP Employee
NXP Employee

HI 宗標 廖

i.MX6 can not be used as a USB charger, but it can

detect that it is connected to external charger.

USB Charger detection scheme has been implemented in MX6 BSP.

You can find the codes in "driver/usb/gadget/imx_usb_charger.c"

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

609 Views
宗標廖
Contributor V

igorpadykov

any comment?

0 Kudos
Reply

609 Views
igorpadykov
NXP Employee
NXP Employee

when you connect smart phone to power supply the phone also can be charged,

just properly connecting D+,D-.

The Basics of USB Battery Charging: A Survival Guide - Tutorial - Maxim

0 Kudos
Reply

609 Views
宗標廖
Contributor V

Hi Igor

But when I connect a smart phone to an imx6q board,the phone can be charged.

So what dose it mean by "i.MX SoC has USB charger detection ability, but it has no charging ability."

Best Regards,

ZongbiaoLiao

0 Kudos
Reply