i.MX6DQ EIM clock for asynchronous access.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ EIM clock for asynchronous access.

Jump to solution
1,896 Views
satoshishimoda
Senior Contributor I

Hi community,

We have two questions about i.MX6DQ EIM clock for asynchronous access.

Please see our questions as below.

[Q1]

We want to know the which clock in Table 22-4 (IMX6DQRM Rev.2) is used for async access.

In other words, which clock in Table 22-4 (IMX6DQRM Rev.2) is INT_CLK in Figure 18 (IMX6DQCEC Rev.3).

Would you let me know it?

[Q2]

I found the max frequency for sync access is 104 MHz in EIM Clock Frequency in I.MX6.

Then, how about in async access?

Is INT_CLK max frequency 104Mhz also as written in chapter 4.9.3 of IMX6DQCEC Rev.3?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
1,576 Views
Yuri
NXP Employee
NXP Employee

  The EIM_BCLK is derivative of the INT_CLK, the recent is equal ACLK (AXI clock),
maximum frequency 133 Mhz.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,577 Views
Yuri
NXP Employee
NXP Employee

  The EIM_BCLK is derivative of the INT_CLK, the recent is equal ACLK (AXI clock),
maximum frequency 133 Mhz.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,576 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

Which clock did you mean "ACLK"?

ACLK_CLK_ROOT

ACLK_EIM_SLOW_CLK_ROOT

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1,576 Views
Yuri
NXP Employee
NXP Employee

ACLK_EIM_SLOW_CLK_ROOT

1,576 Views
satoshishimoda
Senior Contributor I

Hi Yuri,

Thank you for your reply.

OK, I got it!

Best Regards,

Satoshi Shimoda

0 Kudos
Reply