i.MX6DQ Android Beam animation issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ Android Beam animation issue.

Jump to solution
2,061 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Android BSP.

When use Android Beam with jb4.2.2_1.0.0, a animation works on the background.

If repeat this animation, android will freeze and reboot without any log.

And if disable watchdog, the issue will be only freeze and reboot is not occurred.

On the other hand, this issue is resolved by jb4.2.2_1.1.0.

So we think some patch resolves this issue, and we want to know what patch do it.

Could you let me know what patch file resolves it?

Best Regards,

Satoshi Shimoda

Labels (3)
0 Kudos
Reply
1 Solution
1,833 Views
SergioSolis
NXP Employee
NXP Employee

It appears to be an issue with the GPU driver.  Is there a reason for not moving to 4.2.2.1.1 ?

You can try the GPU driver from 4.2.2.1.1 in 4.2.2.1.0 (attached).


You can find jb4.2.2_1.1.0 GPU user space binaries in attach, please apply them on your board.

There are five GPU patches in kernel, you can find them in attach, please apply them to jb4.2.2_1.0.0 kernel and re-build the boot.img.

View solution in original post

0 Kudos
Reply
5 Replies
1,834 Views
SergioSolis
NXP Employee
NXP Employee

It appears to be an issue with the GPU driver.  Is there a reason for not moving to 4.2.2.1.1 ?

You can try the GPU driver from 4.2.2.1.1 in 4.2.2.1.0 (attached).


You can find jb4.2.2_1.1.0 GPU user space binaries in attach, please apply them on your board.

There are five GPU patches in kernel, you can find them in attach, please apply them to jb4.2.2_1.0.0 kernel and re-build the boot.img.

0 Kudos
Reply
1,833 Views
jamesbone
NXP TechSupport
NXP TechSupport

SergioSolis, can you please comment?

0 Kudos
Reply
1,833 Views
YixingKong
Senior Contributor IV

SergioSolis, could you help in following the request, or do you need help from others?

Thanks,

Yixing

0 Kudos
Reply
1,833 Views
YixingKong
Senior Contributor IV

SergioSolis, could you help in following the request, or do you need help from others?

Thanks,

Yixing

0 Kudos
Reply
1,833 Views
satoshishimoda
Senior Contributor I

Could you let me know your status?

I would appreciate if you send me a reply as soon as possible.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply