i.MX6DL:iATU register write sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DL:iATU register write sequence

跳至解决方案
1,892 次查看
koichisakagami
Contributor II

Dear community,

We have been developing their product with iMX6DualLite.
We make the device driver for PCIexpress.


In i.MX6 Reference Manual ( MX6SDLRM ) 4443 page,
it says that " Since AXI core is async to the core_clk, the iATU registers
may not be updated while operations are in progress on the AXI
Bridge Slave interface. "

[Question]
In the case of writing to the PCIE_PL_iATURLBA register,
Is it the correct method as follows ?

1. write to the Viewport Register (PCIE_PL_iATUVR).
2. read the Viewport Register (PCIE_PL_iATUVR).
3. if the correct value is read, write to the PCIE_PL_iATURLBA register.
4. if the correct value is NOT read, wait until the correct value is read.
    And write to the PCIE_PL_iATURLBA register.

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,752 次查看
Yuri
NXP Employee
NXP Employee

  Please look at the next thread for recommended sequence.

"i.MX6DL:Inbound address setting behavior (PCIE_PL_iATUVR)"

https://community.freescale.com/thread/336840

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,753 次查看
Yuri
NXP Employee
NXP Employee

  Please look at the next thread for recommended sequence.

"i.MX6DL:Inbound address setting behavior (PCIE_PL_iATUVR)"

https://community.freescale.com/thread/336840

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复