i.MX6D Precharge Timer PRCT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6D Precharge Timer PRCT

4,004件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, 

I'd like to know how to chose the value of PRCT (Precharge Timner) in MMDCx_MDPDC?

Default is disabled, but what will change when this value chose other than default value.

Best Regards,

Sugiyama

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,727件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thanks.

I understood PRCT is for system power saving mode not DDR timing.

Best Regards,

Sugiyama

0 件の賞賛
返信

3,727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  "Auto precharge is a feature that performs the same individual bank PRECHARGE function [...]

without requiring an explicit command".  You look at auto precharge feature explanation on Micron Web. 

Micron Technology, Inc. - 512Mb: x16, x32 Mobile LPDDR SDRAM (Recommended for new designs) 

   In i.MX6 MMDC by default this feature is disabled. This allows to access previous active page, defined

by DRAM row number, without additional clocks for new page activation. So, setting non-default PRCT 

may sometimes cause some performance penalty. But if new memory access is performed for other

DRAM page, one can get additional clocks for previous page precharging.  

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,727件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thank you for the answer. I read Micron Web.

I'd like to confirm. 

I think when PRCT=00 means disable automatic Pre-charge, it use tRP in MMDCx_MDCFG1.

Then PRCT (!=00) is used as Precharge command period at Automatic Precharge instead of  tRP.

Does it means PRCT should be set the same delay value of tRP(value depend on memory) for Automatic Precharge?

Best Regards,

Sugiyama

0 件の賞賛
返信

3,727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the PRCT parameter just defines the period from last activity to precharge command.

(Assuming the data in current active row are not "interesting" more for fast access.)

tRP - Row Precharge Time:
tRP is the number of clock cycles taken between the issuing of the precharge command and

the active command. In this time the sense amps charge and the bank is activated.

tRAS, tRCD, tRP, tRC ? | TechPowerUp 

 So, PRCT and tRP are different parameters. 

Regards,

Yuri.

0 件の賞賛
返信

3,727件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, Yuri,

Thanks.

If Auto Precharge PRTC use, what DDR parameter should refer to?

Best Regards,

Sugiyama

0 件の賞賛
返信

3,727件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I would say, the PRCT is application depended parameter, but - not DDR related.

Regards,

Yuri.

0 件の賞賛
返信

3,727件の閲覧回数
sugiyamatoshihi
Contributor V

Hi, Yuri,

I' sorry I missed spell. It is PRCT.

I confused its value is depend on application because that is described below. I thought it related DDR parameter.

Automatic precharge of all DDR banks to a specific chip select. Can be activated by
configuring ESDPDC fields: PRCT_0 and PRCT_1. Each field determines a value
loaded to a different chip select.

However, according to your comment, does PRCT define how many idle cycle of DDR count before issue DDR Precharge command at the power down sequence?

Best Regards,

Sugiyama

0 件の賞賛
返信

3,725件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Automatic precharge of all DDR banks may be used for power saving, assuming 

active page consume more power.  

Regards,

Yuri.

0 件の賞賛
返信