i.MX6D BSDL File for Boundary Scan Test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6D BSDL File for Boundary Scan Test

4,174 次查看
rodrigoruizfaja
Contributor II

Hello, my Request is if it's possible to Download the BSDL file por a i.MX6D device, the Specific device name is MCIMX6D6AVT08AB. The main propose is to create the Boundary Scan Advanced Test for ICT station and improve the ICT test coverage.

If there is any special site or request to do, I wolul like to know how to apply.

Thanks in advanced.

#i.MX6bsdl‌

标签 (1)
标记 (1)
3 回复数

3,634 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Rodrigo,

Here, you can download the bdsl for MX6DL

i.MX 6DualLite and i.MX 6Solo BSDL File 

Regards

3,634 次查看
rodrigoruizfaja
Contributor II

Hello

Thanks a lot for the shared BSDL, but I'm looking for the MCIMX6D6AVT08AB that is a iMX6 Dual, but the Automotive processor. So when I try to test the device, I found some errors respecting the BSDL.

The first Error is the IDCODE is different respecting the Expected IDCODE.

ID code failure
Possible fail at
Device : VRM~U15
Failure Message: 28317957
Expected: 00011000100100011010000000011101
Actual: 00100001100100011110000000011101

And then the Boundary Register Length is higher than the expected length. with 3 Boundary cells of diference.

Boundary register length failure
Possible fail at
Device : VRM~U15
Failure Message: 28317957
Expected Length : 648
Actual Length : 651

So the BSDL that I'm working is the "MX6DL_TO1.1.bsdl" that is for Dual Lite Processor, but I'm working with the Dual Automorive Processor. and I need the correct BSDL to perform the Tests.

I'll waiting for you Response... Thanks in advanced.

0 项奖励
回复

3,634 次查看
rodrigoruizfaja
Contributor II

Hello. 

I'm using the BSDL file for iMX6 Dual that you saher in the previous response, but maybe this BSDL is not the correct BSDL for the uC of Automotive use. I'm testing the MCIMX6D6AVT08AB with the x1149, and the expected IDCODE and Boundary Register Length are wrong.

I'm using the BSDL "MX6DL_TO1.1.bsdl" But I think this is for the "Dual Lite", and I need the Dual Core but Automotive Processor BSDL.

Here are the results of the Integrity Test:

ID code failure
Possible fail at
Device : VRM~U15
Failure Message: 28317957
Expected: 00011000100100011010000000011101
Actual:      00100001100100011110000000011101

Boundary register length failure
Possible fail at
Device : VRM~U15
Failure Message: 28317957
Expected Length : 648
Actual Length :     651

Could you help me to share the correct BSDL File?

I'll waiting for your response... Thanks in advanced.

0 项奖励
回复